AXIS#.MOTOR.INERTIA

Description

This parameter is the motor inertia. It is used to calculate the default velocity loop tuning gains (AXIS#.VL.KP ).

Context

For more information see Motor.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

kgcm² for rotary motors

Range

0 to 200,000

Default Value

0

Data Type

Float

See Also

N/A

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDOClosed PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Mappable

AXIS1.MOTOR.INERTIA

500bh

11h

Unsigned32

-

1000:1

Read/Write

No

AXIS2.MOTOR.INERTIA

510bh

11h

Unsigned32

-

1000:1

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.MOTOR.INERTIA

6206

183E

Unsigned32

Read Only

-

AXIS2.MOTOR.INERTIA

71742

1183

Unsigned32

Read Only

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.MOTOR.INERTIA

6206

Float

Read Only

-